Part Number: ADS8684
Other Parts Discussed in Thread: INA828
Hi.
Usually we do ADC design with an instrumentation amplifier at the input to read the sensor signals. In the case of ADS8684 it is showing that it has already amplifier section inside the ADC it self. So should I use an external instrumentation amplifier or not?
If yes, How to implement this without adding a negative voltage rail. I found that there is no requirement for negative voltage rail for ADS8684 as it supports voltage range from -10V to +10V. It requires only a 5V supply.