Other Parts Discussed in Thread: AFE58JD48
Dear,
I'm using a AFE58JD48EVM in combination with a TSW14J56EVM. I've got everything working perfectly with the HSDC pro software and the proprietary GUI for the ADC itself. However when I select the : JESD204B, subclass 1, 4 Lanes, Decimation=4 preset from the presets tab it causes that only half (8) of the 16 channels are visible in the HSDC pro software. However I want to use all the 16 channels and use decimation. I also changed the compression to 1 but this did not change the result. This should be possible right? The decimation even lowers the throughput to the FPGA.
Kind regards,
Jan de Jong