This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4222: The interface in serial resistor value

Part Number: ADS4222

 The datasheet requires in serial resistor for CMOS interface to FPGA. how about the value? 10ohm ok?

1) interface of data output

2) interface of spi

  • Xiaoqiang,

    I would suggest using any value between 10 and 22 Ohms for the data lines and place these as close as possible to the ADC. For the SPI, I would only use a resistor for the clock (10-22 Ohms) and place it close to the ADC.

    Regards,

    Jim