Part Number: ADC3244EVM
Other Parts Discussed in Thread: THS4541
Hi team,
Please help the customer with issue bellow.
I want to use THS4541 differential amplifier onto the board to amplify my input signal by the gain 10 V/V. To do this, I will first modify the board to arrange it in DC-coupling mode. I will make the modifications given in the board datasheet, Table 6 (on page 13). I am also putting this table at the attachment.
Afterwards, to set the gain of the amplifier to 10, I will change the resistor R98 with 170 Ohm, R92 with 23.6 Ohm and R93 with 35 Ohm. I will switch the position of jumper SJP1 to 1-2. Therefore, R96 and R97 will be in parallel which results 27 Ohm and my total termination resistance value will be 35+27 = 62 Ohm. So, I will achieve the resistance values for gain 10 V/V which is given on Table.1 of THS4541 datasheet on page 23. I am also putting the schematic of THS4541 and the gain table at the attachment.
Please could you confirm my approach?
B.R.
Eric