Part Number: ADS1261
Other Parts Discussed in Thread: , ADS1235
Dear all,
I am trying to use an ADS1261 in AC Excitation mode to read two full Wheatstone Bridges. Thus, I am planning to use AIN0 and AIN1 as REFP0 and REFN0, and use AIN2 and AIN3 as REFP1 and REFN1. The AC Excitation is 2 wire and then use the pairs ANI6 - AIN7 and AIN8 and AIN9 as differential inputs for each bridge.
The schematic that I came across with is as follows, but I not sure of it and I also have some doubts:
1) - the AINCOM must be connected to some signal or can be left floating?
2) - the REFOUT must be connected to 5V? or should I use the 2.5V. The bridge is being powered with AVDD = 5V and DVDD = 3.3V for the MCU


Thanks in advance,
Miguel