The DS isn't clear, but the note below DS table 26 says: "(1) The actual VREFby2 value may vary by ±10% from Table 26."
Does this mean that the min/max of the Vrefby2 is ±10% from Vref/2? I assume this is not correct. Please provide the accuracy of the Vrefby2 output which would be a combination of the divider tolerance and offset voltage. If this is trimmed during production, is it reflected in the DS somewhere and I'm just missing it? Thanks- Mark.