This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: SYSREF - NCO MODE

Part Number: DAC38J84

I am working with DAC38J84 in NCO mode in the following way:

1. set a new frequency through SPI (registers 0x14 - 0x16)

2. using a one sysref pulse to update the NCO ( 0x1E = 2222 , 0x1F = 2220)

DAC_CLOCK = 1920MHz

SYSREF WIDTH = 500psec

DAC configuration is attached

0x00	0x0218
0x01	0x0003
0x02	0x2050
0x03	0xA300
0x04	0xF0F0
0x05	0xFF07
0x06	0xFFFF
0x07	0x3100
0x08	0x0000
0x09	0x0000
0x0A	0x0000
0x0B	0x0000
0x0C	0x0400
0x0D	0x0400
0x0E	0x0400
0x0F	0x0400
0x10	0x0000
0x11	0x0000
0x12	0x0000
0x13	0x0000
0x14	0x0000
0x15	0x0000
0x16	0x4200
0x17	0x0000
0x18	0xAAAA
0x19	0x52AA
0x1A	0x0020
0x1B	0x0000
0x1E	0x2222
0x1F	0x2220
0x20	0x2022
0x22	0x1B1B
0x23	0x01FF
0x24	0x0010
0x25	0x4000
0x26	0x0000
0x2D	0x0001
0x2E	0xFFFF
0x2F	0x0005
0x30	0x0000
0x31	0x1000
0x32	0x0000
0x33	0x0000
0x34	0x0000
0x3B	0x3800
0x3C	0x0228
0x3D	0x0088
0x3E	0x0108
0x3F	0x0000
0x46	0x1882
0x47	0x01C8
0x48	0x3143
0x49	0x0000
0x4A	0x001E
0x4B	0x0801
0x4C	0x0903
0x4D	0x0300
0x4E	0x0F0F
0x4F	0x1C61
0x50	0x0000
0x51	0x00DC
0x52	0x00FF
0x53	0x0000
0x54	0x00FC
0x55	0x00FF
0x56	0x0000
0x57	0x00FF
0x58	0x00FF
0x59	0x0000
0x5A	0x00FF
0x5B	0x00FF
0x5C	0x1133
0x5E	0x0000
0x5F	0x3210
0x60	0x5764
0x61	0x0211
0x64	0x0001
0x65	0x0001
0x66	0x0001
0x67	0x0001
0x68	0x7709
0x69	0x0000
0x6A	0x0000
0x6B	0xBD07
0x6C	0x0007
0x6D	0x0090
0x6E	0x0000
0x6F	0x0000
0x70	0x0000
0x71	0x0000
0x72	0x0000
0x73	0x0000
0x74	0x0000
0x75	0x0000
0x76	0x0000
0x77	0x0000
0x78	0x0000
0x79	0x0000
0x7A	0x0000
0x7B	0x0000
0x7C	0x0000
0x7D	0x0000

SYSREF PULSE:

For each sysref trigger a different result is obtained.

for example, when i set the dac output to 495MHz i got the following result:

good output - low spurs:

 

bad output - high spurs (sometimes even higher than my desirable signal):

when i use a SIF SYNC trigger instand of sysref , everything works fine.

Please advise what is wrong with my configuration?

Thanks,

Asaf