Part Number: ADC3664EVM
Other Parts Discussed in Thread: ADC3664, ADC3644, CDCE6214
Hello E2E,
Our customer are evaluating for performance of ADC3664 on EVM.
They would like to experiment with the 125MHz 2-wire method and the 65MHz 1-wire method. Is there a way to input the clock without using the SMA connector?
They checked the schematic, but didn't know how to input two clocks from the FMC connector, and thought that the on-board clock generator wasn't good enough to generate DCLKIN.
Regards,
ACGUY