Part Number: ADS1258
Other Parts Discussed in Thread: ADS131M08
Dear Expert
As for ADS1258, our company used this chip to do a project of 8 channels of 2KHz sampling frequency (that is, the sampling frequency of each channel is 16KHz). Now the project has a new requirement -- to use ADS1258 chip to achieve 8 channels of above 16KHz sampling frequency.
1.According to the chip manual and actual test verification, the maximum sampling frequency of a single channel of ADS1258 in the automatic scanning mode is 23.7KHz, which is consistent with my requirement -- a total of 16KHz sampling frequency of 8 channels (means the sampling rate to save a single channel is:8* 16KHz = 128KHz) is far away. Is there any way to solve it?
2.In addition: Although it has been measured and stated in the manual, I still want to confirm whether the maximum sampling rate of 23.7kSPs in the automatic scanning mode is the highest sampling rate for a single channel. Is there any method to make the total sampling rate of 23.7kSPs for multiple channels?Also want to know, at 16MHz external crystal oscillator, SPI clock signal SCLK frequency can support to how much Hz?