Other Parts Discussed in Thread: ISO7141CC
Hi,
We have developed our 4-20 mA loop current module that uses the DAC161S997 and it is working fine.
We have been able to communicate using the HART protocol, however with a critical limitation. When the current loop is below 5 mA, the HART signal is severely attenuated, we can only communicate within the range of 5-20 mA, which is not acceptable in most industrial processes.
Could you give us any insight on what is the cause of the problem or a suggestion regarding the circuit connections to our module. Please find in the attachments the circuit diagram of our module.We are using a fintHRT T210 HART interface module directly into the 4-20 loop (pins 2 and 5 from CN1).
Thank you.