Part Number: DAC81416
Hi
DAC output is 0V. I have used the following code
Write 0x0A 0x0000 // Configure for 0 to 5V
Write 0x03 0x0A84 // Device in active mode
Write 0x04 0x3F00 // Enable Internal Reference
Write 0x09 0x0000 // Power up all channels
Write 0x10 0x7FFF // Write mid code to DAC 0
Write 0x1F 0xFFFF // Write full code to DAC 15
Pins Configured as
Toggle0 = Toggle1 = Toggle2 = Gnd
LDAC = RESET = CLR = VIO (5V)

SPI lines
Thanks in Advance.