Part Number: AMC7834
Hi,
I'm working with an implementation of this chip where there is a 'race condition' of sorts between the xVDD, AVCC and IOVDD pins, and the ADC MUX inputs. Basically, an unregulated supply is applied to the board, which is then regulated to power the AMC7834, but the AMC7834 is also connected to measure this unregulated supply through both its current and voltage mux inputs. This means that it is likely that voltage will be applied to these inputs before the AMC7834 is powered itself.
I couldn't see any specific mention of whether this was something to avoid, or not, in the data sheet, so I thought I would ask here if this was a problem.
Regards,
LT