Part Number: ADS54J60EVM
Other Parts Discussed in Thread: ADS54J60
Hello TI Team,
I am currently working on an acquisition setup involving a pulse generator and a TSW14J56 with an ADS54J60EVM.
My application requires to acquire several millions samples in a burst, synced with a clock from the pulse generator. From the datasheet of the ADS54J60 it appears that the minimum sampling frequency is 250 MHz, but I have been able to make it work at 122.88 MHz using the corresponding firmware.
However, the sampling rate I need is much lower, with a sample very 500 ns to 2 us. What attracted me to the TSW14J56 was the USB3.0 and large RAM available, which would maximum data transfer to the computer.
Is there a way to have this kind of low sampling rate, maybe by skipping some samples either loaded to the RAM or transfered to the PC ?
Is my system way oversized for my application and if this is the case, what would be the configuration you would recommend ?
Thank you in advance,
Best regards.