Hi,
I need a high-speed DAC with very low residual 1/f phase noise.
Maximum clock rate should be at least 200MHz, 400MHz or higher would be nice.
Resolution should be at least 14-bit, 16-bit preferred.
Data interface should be LVDS or CMOS. DDR interface is OK if it can transfer one data sample per clock cycle. JESD204B is kind of OK if it is able to run with 40MHz DAC clock frequency.
Residual phase noise (assuming a noise-free clock signal and supplies run from virtually noise-free batteries) at 100Hz fourrier frequency and 20MHz output frequency should not be higher than -150dBc/Hz.
Is there anything from TI that would match these requirements?
Thanks,
Whisp