Part Number: ADS4229
Other Parts Discussed in Thread: THS4541, , LMH5401
Concernig Vocm, and suitable fast differential amplifier on input.
I chose the THS4541 differential amplifier, because of its excellent performance. This amplifier has a lower limit on the Vocm of 0.95V.
The ADS4229 Vocm specification is 0.95V, unless it is clocked faster than 160MHz, in which case it changes to 0.87V, which means that I cannot directly couple the ADC and the differential amplifier.
I need to couple the amplifier and the ADC with a DC offset, because my signal is unipolar and if AC coupled I would lose half of the ADC range, complicating the rest of my design.
Can you propose another differential amplifier that can work with the 0.87V Vocm? Running off 3.3V with a bandwidth of 200MHz and a slew rate above 200V/us, preferably faster.
What would be the effect if I sacrifice the 80mV difference on common mode and just allow for a smaller signal swing? ie I run the amplifier at 0.95V and the ADC at 0.87V.
Any help would be appreciated. If any other solutions exist, please make suggestions.