Other Parts Discussed in Thread: DAC37J84
Hi~
When DAC37J84 is used to change the sampling rate,JESD204B protocol can be established at sampling rates 1200MSPS 1000MSPS 600MSPS 500MSPS, but cannot be established at sampling rates below 500MSPS(400MSPS 300MSPS 250MSPS 240MSPS 200MSPS)
The specific performance is as follows: the protocol establishment of CGS, ILAS and User Data Transmission is completed at first, and then the establishment of User Data Transmission fails after waiting for a few seconds. After that, the sync signal sometimes lowers a pulse, sometimes few nanoseconds, resulting in the unstable establishment of the protocol, as shown in the following figure.





My DAC configration in 200MSPS sampling rates is below
FPGA:XCKU040-FFVA1156-2-i
L M F S HD: 8 4 1 1 1
DAC input rate: 200MSPS
Lane rate: 2Gbps
Interpolation: 1x
I added configuration below.
8'hFF,16'h0000
8'h00,16'h0018
8'h01,16'h00A3
8'h02,16'h2002
8'h03,16'hA300
8'h04,16'h0000
8'h05,16'hFF03
8'h06,16'hFFFF
8'h07,16'h1E00
8'h08,16'h0000
8'h09,16'h0000
8'h0A,16'h0000
8'h0B,16'h0000
8'h0C,16'h0400
8'h0D,16'h0400
8'h0E,16'h0400
8'h0F,16'h0400
8'h10,16'h0000
8'h11,16'h0000
8'h12,16'h0000
8'h13,16'h0000
8'h14,16'h0000
8'h15,16'h0000
8'h16,16'h0000
8'h17,16'h0000
8'h18,16'h0000
8'h19,16'h0000
8'h1A,16'h0020
8'h1B,16'h0000
8'h1E,16'h9999
8'h1F,16'h9980
8'h20,16'h8008
8'h22,16'h1B1B
8'h23,16'h01FF
8'h24,16'h0020
8'h25,16'h2000
8'h26,16'h0000
8'h2D,16'h0001
8'h2E,16'hFFFF
8'h2F,16'h0004
8'h30,16'h0000
8'h31,16'h1000
8'h32,16'h0000
8'h33,16'h0000
8'h34,16'h0000
8'h3B,16'h0800
8'h3C,16'h0028
8'h3D,16'h0088
8'h3E,16'h0108
8'h3F,16'h0000
8'h46,16'h0120
8'h47,16'h3450
8'h48,16'h31C3
8'h49,16'h0000
8'h4A,16'hFF01
8'h4B,16'h1200
8'h4C,16'h1F07
8'h4D,16'h0300
8'h4E,16'h0F6F
8'h4F,16'h1C61
8'h50,16'h0000
8'h51,16'h00DC
8'h52,16'h00FF
8'h53,16'h0000
8'h54,16'h00FC
8'h55,16'h00FF
8'h56,16'h0000
8'h57,16'h00FF
8'h58,16'h00FF
8'h59,16'h0000
8'h5A,16'h00FF
8'h5B,16'h00FF
8'h5C,16'h6666
8'h5E,16'h0000
8'h5F,16'h0123
8'h60,16'h4567
8'h61,16'h0211
8'h64,16'h0000
8'h65,16'h0000
8'h66,16'h0000
8'h67,16'h0000
8'h68,16'h0000
8'h69,16'h0000
8'h6A,16'h0000
8'h6B,16'h0000
8'h6C,16'h0000
8'h6D,16'h0000
8'h6E,16'h0000
8'h6F,16'h0000
8'h70,16'h0000
8'h71,16'h0000
8'h72,16'h0000
8'h73,16'h0000
8'h74,16'h0000
8'h75,16'h0000
8'h76,16'h0000
8'h77,16'h0000
8'h78,16'h0000
8'h79,16'h0000
8'h7A,16'h0000
8'h7B,16'h0000
8'h7C,16'h0000
8'h7D,16'h0000
8'h4A,16'hFF1E
8'h4A,16'hFF1F
8'h4A,16'hFF01
RBD has been adjusted 8, 16, 24, 28 and 32, but this problem still exists below the sampling rate of 500MSP
After reading the registers 0x64~0x6B, it is found that if the value is above 500MSPS, it is 0000. if the value is below 500MSPS, there are three possibilities as follows: 0002, 0100 and 8100, but the cause of the problem cannot be located
In addition, since FPGD_DCLK and GTH CLK need to switch as the sampling rate changes, the FPGA constraint constrains these two clocks to a sampling rate of 1200MSPS (below), not sure if this will cause a problem (in fact, We tried to constrain it to 200MSPS with the FPGD_DCLK and GTH CLK clock constraints, both of which are 100MHz, but the protocol for 200MSPS cannot be established.)
Create_clock-period 3.333-name jesd204_dac_refclk [get_ports refclk0p]
Create_clock -period 1.667-name GLBLCLKP [get_ports GLBLCLKP]
In addition, the maximum line rate in this design is 12Gbps, but the FR4 material is used. It is uncertain whether it will cause problems (but if it is the material problem, why is the establishment of high frequency protocol normal while the establishment of low frequency protocol failed).
Thank you for your help