Part Number: TLC3541
We have been experiencing failures of the TLC3541ID ADC in 15% of our boards. The parameters of the design are; REF=5V, VDD =5.2V, FS is tied to VDD, AIN can be a maximum of 5.3V. Test engineers have stated that the device fails immediately and they can't retrieve good data from the SPI interface. They have mentioned that SDA actually mirrors SCLK after the failure. We have noticed that the CS line comes up before VDD has reached a steady 5.2V. Could that be an issue?
Thanks for any input.