Hi,
I am able to read and write registers of the ADC.
Configuration for the ADC :
1) Changing the sampling rate to 100sps from 20sps(default)
2) Changing the input mux bits of register(10h) to AIN0 to AINCOM as shown in the attached figure.

3) External reference is enabled in the design as shown in the attached figure.

I have set the PGA gain as 0.125 and given the 5.00v as an input to the ADC.I am getting the x"ecxxxx" hexadecimal value as the ADC conversion output .
I had attached the screenshot of our schematic and waveform from the vivado ila.