Other Parts Discussed in Thread: ADS1247, ADS1294, ADS1194, TMS320F28335, MSP430F2274, ADS1298, MSP430F2013
Hi,
is ADS1247 suitable for a 2 or 3-lead 3.6V Li-Po battery powered single supply ECG? If it is, which way is to follow when conditioning the electrode signals:
a. feed the lead signals into the differential inputs via simple RC antialiasing filter (only 2 leads this way), with PGA at G=5...10;
b. convert the differential signal to single ended with an INA (G=5...10, single supply, REF pin at mid supply) then option a. with/without additional PGA. This way ADS1247 gives 4 channels.
c. convert the differential signal to single ended with an INA (G=5...10, single supply, REF pin at mid supply), AC couple using a 0.05Hz RC HP filter with a level shift of 20-50 mV then option a. with/without additional PGA
Thank you.