Part Number: DAC38RF82EVM
Thanks in advance for your help.
I am using a DAC38RF82EVM to generate two channel waveforms and I'm controlling it with a TSW14J56EVM. If possible, I would like to be able to disable the DAC output without powering down the board. (I'm using this in an experimental setup and often need to verify my signals on a scope or spectrum analyzer.) I see from the user guide for the DAC board that jumper J2 can be positioned so as to enable or disable the DAC output (p3, table 2, row 2). Can this be changed while the board is running or is it for operating in some other mode and only to be changed when the board is off. Even better is it possible to disable and reenable the DAC output via SW?
Thanks again,