Part Number: ADS1278-EP
Hi E2E,
Good day.
Based on the datasheet, the SCLK may be either in free-running or stop-clock operation between conversions. Other than power consumption, is there any difference in the device performance?
Also, the SPI format is limited to a CLK maximum input frequency of 27 MHz. What will happen if the SPI format is used above 27 MHz instead of Frame-Sync format?
It was also mentioned that as with any high-speed data converter, a high-quality, low-jitter clock is essential for optimum performance. What will happen to the device if does not use a high-quality,low-jitter clock?
What implementation can be used for application demanding of frequency change about every 20ms to ensure same number of samples every cycle?
Regards,
Carlo