Part Number: ADC3664
It seems like the default output format is 14-bits in 2s complement and the DDC is bypassed. I can't quite figure out the default configuration for the number of lanes used. I'm trying to understand if my desired application can work without any SPI configuration or not.
What is the default output format, number of lanes used, FCLK, serialization, etc?
This would be nice to make explicitly clear in the datasheet.