Part Number: TSW1400EVM
Other Parts Discussed in Thread: AFE5818EVM, AFE5818
Hello.
I am using the HSDCPro software to interface with the TSW1400EVM which is connected to the AFE5818EVM module through the LVDS connector.
I am injecting a frequency swept sine wave into the AFE5818EVM module and am using the "Continuously Capture" option in the HSDCPro software to capture the swept sine wave. I am doing this on the "Single Tone" setting to capture the peaks of the swept sine wave over a range of frequency . This is to verify filter responses (high pass / low pass) in the signal chain (including the high pass and low passes created inside the AFE5818). The goal is to have a somewhat magnitude plot of the frequency response.
There is an option to "Write Captured Data to File" in the "Data Capture Options" tab in the GUI. I am wondering where this data file gets created and stored on my PC and what data it is storing? Will I be able to get my "Single Tone" data that I capture every time a continuous capture sample is taken? Or does it just log the latest capture and then get overwritten?
The only place I can see a file get created is under C:\Users\Public\Documents\Texas Instruments\High Speed Data Converter Pro\ where there is a "FFT Data.bin" file that gets created.
Any help with this would be greatly appreciated.
Thank you!