Part Number: ADS1282-HT
Other Parts Discussed in Thread: ADS1282, ADS1281
Hello,
I want to have on the same SPI, the ADS1282 and a DAC (AD5600) - sharing the same SCLK and DIN.
The problem is that the ADS1282 doesn't have a Chip Select and if I send data to the other SPI device (AD5600), it takes commands/data on the DIN.
I have a few options but I don't know if they are doable or what is the best one:
1 - disable the ADS1282 CLK
2 - hold in reset the ADS1282
3 - neglect the effect of sending data on the same SPI to the DAC - hooping that it doesn't change anything in the ADC1282
4 - use a different SPI - not preferred
Question: How can I disable the ADS1282 when I send data to the DAC?
Thanks,
Marius Raducanu