This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC112: DVALID Signal

Part Number: DDC112

Hi Team, 

Having a chain of DDC112, it is 4 PCB, each of its contain 8 DDC112 chips. For control of this structure they use MCU (stm32), In reference on the datasheets for DDC112  control scheme is correct, but there are 2 issues all time:


1) DVALID signal occurs from 370 microseconds, but it must occur from 421 usec for First conversion and 454 usec for the second.

2) When they use test mode they get the same result for each side A and B, but I set different charges for each side. For A it is 1 charge (13pC), for B side it is 3 charge (39pC), but the result of the integrated circuit is the same for all sides.


A little bit about using scheme: it is non-conversion mode, 50 microseconds integration time, 300 Hz frequency of integration, 10 MHz of CLK, and 6.25 MHz of DCLK. In their opinion, the First problem occur because of power-up problems

Hoping for your inputs.

Thank you.

-Mark