Part Number: ADC12D1000
Hi,
we are using the ADC12D1000 in a mature product and have a question regarding the reference voltage output VCMO:
In the datasheet, it is specified to vary from 1.15V to 1.35V with a typical value of 1.25V.
Are there any data on the statistical distribution of this voltage or the probability to reach the min max voltages?
it is slightly temperature dependent 6mV over Tmin=-40 to Tmax=85 and considering 1.25V.
The rest of the VCMO variation is probably due to the process corners since it appears to be a bandgap voltage.
Thanks,
Alen