Other Parts Discussed in Thread: THS4551, OPA2625, ADS127L11
I want to digitalize an analog signal with the mentioned ADC. Then feed the digital data to an FPGA (XILINX ARTIX 7 {xc7a35ticsg324-1L}).
That means the ADC will be the slave (i see no other option). What should I feed the ADC as an input ? when I only want its conversion (the output).
How do I avoid saving the conversion result and just drive it directly to one of the outputs ? And at what sclock frequency should I use if my FPGA-clock is 100MHz ?
I just want the simplest ADC out of this device, so how do I do it ? and which pins (not involved in the SPI standard protocol) should I connect with the FPGA ?