Part Number: ADC12DJ3200
Hi team,
The customer uses jmode13 with 15bit effective bits. After 32-bit data is received, it is disassembled into I and Q channels with 15bit each:

The swing measured at the single end of AD input is 262mv, and the difference is 524mv. Set FS_RANGE to 2000, there will be no clipping, and the maximum value of the collected data is 10000 (far from 16384); Set FS_RANGE bit 0020 is theoretically out of range, but the maximum collected data is only 10200. What may be the reason?
The waveforms captured by the above two settings are ideal sine waves
The data to be checked is channel I. Will the amplitude of channel I or channel Q be 1/2 of the input signal after digital orthogonal down convert?
Best Regards,
Amy Luo