Part Number: ADS1258-EP
Other Parts Discussed in Thread: ADS1258
Hello,
What are the specific jitter requirements for the ADS1228-EP's external clock input? The datasheet only says, "Make sure to use a clock source clean from jitter or interference;" I was hoping you all could provide more specific requirements. I'd like to use my FPGA's PLL output as the external clock source, but it has a worst case jitter of 2.5% × clock period peak-to-peak period, so I'm not sure if that's "clean" enough for this ADC. Thanks!
Cheers, Danielle