Part Number: ADS1263
Other Parts Discussed in Thread: ADS1262,
Hello Guys,
Good day.
Our customer is using 40PC150G2A (Pressure sensor), honeywell for sensing pressure. They are looking for an ADC best suited for their application. are upgrading our gas chromatography machine. They need : 0.1 kPa (0.001 psi) resolution, Max 150 psi and accuracy of < ± 2.0 % (full scale).
They have initially bought ADS1263IPW for this application. Is this suitable for the said sensor? See below.
40PC_Series_Pressure_Sensor_Honeywell.pdf
Thanks and regards,
Art