This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L11EVM-PDK: Spectrum Analysis of High Speed Mode and Low Speed Mode

Part Number: ADS127L11EVM-PDK


Hello Team,

I have a question about GUI. *Attached the capture

I have input the following signals, but the results are quite different in high speed mode and low speed mode.

-frequency: 1 kHz

-waveform: sinusoidal

-amplitude: ±0.834 V

In high speed mode, the first harmonic is set to 1kHz, but in low speed mode, 125Hz (one eighth of 1kHz) is caught as the first harmonic.

Since low speed mode is one eighth of the sampling of high speed mode, it seems to be related. I also notice that THD is extremely worse than in High Speed mode.

Please let me know what you think.

Regards,

Masakazu