Other Parts Discussed in Thread: ADS7881, AM3703
Hello-
Regarding the ADS7881 12b SAR. My cusotmer is trying to use it between a contact imagesensor and a AM3703 based SoM. His question:
"Is it safe to assume that the voltage that gets converted to digital is the actual voltage present at the analog input the instant /CONVST transitions from low to high (at either 50% or 90% threshold) ?
The reason I am trying to get a better understanding is because we are going to need to pick a time where our analog data is stable.
I have included my own timing diagram and also included an actual screenshot. See attachment. The 3rd waveform is representative of output from contact image sensor. I would like to sample the analog signal at input to ADC at time (1).
I am also thinking it would be best to read 12 bit data at time (1) so we would send this signal to the AM3705 CAM_PCLK input."
Thanks and best regards,
Tim Starr on behalf of JY