Part Number: DAC80502
Hello,
I am trying to use the DACx0502 in my design. Reading the documentation, it is not clear whether SYNC pin can remain low between consecutive frames.
In particular, the use case I am thinking of is to set DAC1 and DAC2 data first, then followed by a write to the LDAC register, which is 3*24bit in total. Do I have to raise the SYNC pin high between each 24bit transfers or can I allow it to remain low between transfers? It is more convenient to write the software if they can remain low between consecutive SPI frames.
Thanks!