Other Parts Discussed in Thread: TVP5151
I'm trying to interface a TVP5151AM1 with a Broadcom MPEG decoder that accepts BT.656 input. We've found the I2C interface inadequate and are getting dropped data even using FIFO mode. The Broadcom supports a number of ancillary data formats including several variants of SAA7113, SAA7114 and SAA7115. They also support SMPTE 291M Type 1 & 2 formatted data. The TVP5151 seems to output a proprietary format that looks a little like 291M ANC, but uses even/odd parity bits even though the output is not 10-bits. Is it possible to put the TVP5151 in a compliant SMPTE 291M mode?