Part Number: DAC81416
Other Parts Discussed in Thread: ENERGIA
Dear TI,
We are using DAC81416 dac IC in our design.
Can you please provide the Linux driver source code for this chipset?
Regards,
Shilpa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please allow us a day's time for the header files. Also Please find the spi code examples for energia sketch.
#include <SPI.h>
#define NUM_BYTES 3 //Number of bytes in SPI frame
//SPIClass tivacSPI0(0); // SSI0
//SPIClass tivacSPI1(1); // SSI1
//SPIClass tivacSPI2(2); // SSI2
//SPIClass tivacSPI3(3); // SSI3 on port F
SPIClass tivacSPI3_Q(4); // SSI3 on port Q
void setup() {
uint8_t initTx0[NUM_BYTES], initTx1[NUM_BYTES], initTx2[NUM_BYTES], i;
int8_t ret;
uint8_t *initPtr;
Serial.begin(9600);
Serial.print("Starting DAC81416 Example");
//tivacSPI0.begin();
//tivacSPI1.begin();
//tivacSPI2.begin();
//tivacSPI3.begin();
tivacSPI3_Q.begin();
pinMode(PD_2, OUTPUT); // Configure PD2 as CLR
digitalWrite(PD_2, HIGH); // set CLR HIGH by default
//Range: +/- 20V
initTx0[0] = 0x0A;
initTx0[1] = 0xCC;
initTx0[2] = 0xCC;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Range: +/- 20V
initTx0[0] = 0x0B;
initTx0[1] = 0xCC;
initTx0[2] = 0xCC;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Range: +/- 20V
initTx0[0] = 0x0C;
initTx0[1] = 0xCC;
initTx0[2] = 0xCC;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Range: +/- 20V
initTx0[0] = 0x0D;
initTx0[1] = 0xCC;
initTx0[2] = 0xCC;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Power-up device
initTx0[0] = 0x03;
initTx0[1] = 0x0A;
initTx0[2] = 0x84;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Power-up all channels
initTx0[0] = 0x09;
initTx0[1] = 0x00;
initTx0[2] = 0x00;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Enable Broadcast for all Channels
initTx0[0] = 0x05;
initTx0[1] = 0xFF;
initTx0[2] = 0xFF;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
//Write Code to all Channels
initTx0[0] = 0x0F;
initTx0[1] = 0xFF;
initTx0[2] = 0xFF;
initPtr = &initTx0[0];
ret = tivacSPI3_Q.DACtransfer((uint8_t*)initPtr, (uint8_t)NUM_BYTES);
}
void loop() {
int8_t rv, ldacFlag = 0;
int32_t sampleCount;
uint8_t *txPtr;
uint8_t spiTx0[NUM_BYTES];
//Write Mid-code
spiTx0[0] = 0x10;
spiTx0[1] = 0x7F;
spiTx0[2] = 0xFF;
txPtr = &spiTx0[0];
rv = tivacSPI3_Q.DACtransfer((uint8_t*)txPtr, (uint8_t)(NUM_BYTES));
delay(100);
//Write Full-code
spiTx0[0] = 0x10;
spiTx0[1] = 0xFF;
spiTx0[2] = 0xFF;
txPtr = &spiTx0[0];
rv = tivacSPI3_Q.DACtransfer((uint8_t*)txPtr, (uint8_t)(NUM_BYTES));
delay(100);
}
//Addition to SPI.cpp
int8_t SPIClass::DACtransfer(uint8_t* datapointer, uint8_t numBytes) {
unsigned long rxtxData[MAX_BYTES];
if(numBytes > MAX_BYTES){
return -1;
}
if(datapointer == NULL){
return -1;
}
for(int byteCount=0; byteCount < numBytes; byteCount++){
rxtxData[byteCount] = datapointer[byteCount];
}
if(SSIBitOrder == LSBFIRST) {
return -1;
}
for(int byteCount=0; byteCount < numBytes; byteCount++){
ROM_SSIDataPut(SSIBASE, (uint8_t) rxtxData[byteCount]);
}
while(ROM_SSIBusy(SSIBASE));
return (int8_t) 0;
}
In case, you need a generic setting for SPI on any processor. It's as follows:
Mode: Mode-1 (CPOL=0, CPHA=1)
Order: MSB First
CS Polarity: Active Low
Number of Bytes: 3
You can use GPIOs for LDAC and CLR, if needed.
Regards,
AK