Other Parts Discussed in Thread: AFE7900, AFE7950, AFE7903, AFE7906
Hi
Can you suggest any DAC that supports JESD204C Protocol ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Can you suggest any DAC that supports JESD204C Protocol ?
Jim,
I have developed my Custom JESD204C Tx and Rx IP's which can support 64B66B CRC 12, CRC 3 and FEC Modes
Now I want to test my IPs on TI EVM's
My Requirements :
1. EVM (Tx and Rx) must support FEC Mode.
2. Must be tested at High Data Rates above 24 Gbps.
Transceiver AFE7900 and AFE7950
1. Does these support FEC Mode and High Data Rates
2. In the Datasheets of AFE7900 and AFE7950, Nothing is mentioned about FEC mode...Can you provide detailed Datasheets of these transceivers ?
Hi Pavan,
You can request access to full datasheets of AFE7900 and AFE7950 in the product web-pages. By clicking 'Request now' link shown below:
Link for the same:
Regards,
Vijay
Hi Vijayendra Varma,
1. I have requested for the full datasheet of AFE7900.
2. Does this Transceiver support SERDES rate above 24 Gbps ?
3. Also What is the basic difference between EVM of this transceiver and EVM of ADC/DAC ?? Does ADC/DAC EVM provide any additional features ?
Hi Pavan,
2. Yes. AFE79xx supports SERDES rates above 24Gbps.
3. AFE79xx has multiple DACs and ADCs integrated into it. This EVM supports evaluation of both ADCs and DACs.
Regards,
Vijay
Hi Vijayendra Varma,
Thanks for your support, I will go through the AFE7900 documents
Hi Vijayendra Varma,
I got access for Datasheets of AFE7900, AFe7950, AFE7906, AFE7903.
But in all these Datasheets, there is no information about FEC Mode in 64B66B Encoding.
I think only CRC 12 and CRC 3 are supported.
So Can I assume that FEC mode is not supported by these Transceivers ?
Can you suggest any DAC which supports JESD204C FEC Mode and SERDES RATE more than 24 Gbps ?
Hi Pavan,
You are correct. The AFE79xx doesn't support FEC in 64b66b encoding mode.
We don't have any released devices with DACs that support FEC.
regards,
Vijay
Thanks for the information Vijayendra Verma
I have developed my Custom JESD204C Tx and Rx IP's which can support 64B66B CRC 12, CRC 3 and FEC Modes
Now I want to test my IPs on TI EVM's
My Requirements :
1. EVM (Tx and Rx) must support FEC Mode.
2. Must be tested at High Data Rates above 24 Gbps.
Any suggestions ?
Hi Pavan,
The only DAC that goes beyond 24Gbps JESD lane rate is available in AFE79xx. But this does not have JESD 204C FEC mode. So there's no TI part available to support this mode. I apologize for the inconvenience
Regards,
Vijay