Part Number: ADS1247
After a Sync Command is sent (04h) with a PGA setting of 160 SPS, the spec indicates that data will be ready 6.240mS after.
If I send RDATA (12h) after 6.240mS from the sync, will I have to wait another 6.240 mS to get an accurate reading?
So order is
sync (0x04)
wait 6.240 (actually waiting 9 ms)
RDATA (0x12)
can I expect valid data at this point or would I have to wait again?
Thank you,
George