Part Number: ADS42LB69
Hi,
I'd like to feed ADS42LB69 clock input as LVDS from LMK 4828. I already have ac coupling capacitors of 100nF at the output of LMK; therefore, do I still need to put ac coupling capacitors at the clk inputs of the ADS42LB69 as shown in Figure 118 of the datasheet of the ADC revised on May 2016?
One other question is about the termination resistance of 100ohm placed at the clk inputs of ADC, In Figure 118 of the datasheet, ac coupling capacitors are put after(closer to the ADC) the termination resistance of 100 ohm. Is this correct? Do we not need to put the termination after ac coupling capacitors?
My last question is about the 560 ohm termination resistance that needs to be put at the HSDS/LVDS output of LMK. Doesn't this resistance interfere with the 100ohm that's put at the ADC side clk input?
Thanks for your help in advance.
Regards.