This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF42: adc32rf42

Part Number: ADC32RF42

Hi,

I have a simple question:). Does ADC32RF42 run at 14 bit bypass mode at fs=1.5GHz?

In Table 13 on page 46, it says max freq at 14 bit bypass mode is 1.25GHz. 

On page 6, on top of the table test condition says 14 bit, bypass mode, fs=1.5GHz.

Which one of the above 2 statements is correct?

Thank you.