Part Number: ADS7828
I'm using the ADS7828EB/2K5 device. My power supply is 3.3V at pin 16 (VDD+) and my reference voltage at pin 10 (REFIN/REFOUT) is 3.1V. My concern is this: if I turn of the power supply 3.3V at pin 16 and the reference voltage is still ON. Is this going to damage the chip or not. I test it out after I turn the supply off and ON again the device works normally but I want to make sure this will not cost damage to the device later ON.
Please advice.