Part Number: AMC3336EVM
Other Parts Discussed in Thread: AMC3336
I am testing with a AMC3336EVM to see how to read the value detected. I am varying a 1.0V signal between INP and INN, but when I send the chip 16 clock cycles the value received on DOUT varies widely between read attempts for the same voltage.
My setup is that I am hooking INP and INN directly to the power supply that is supplying a 0.9V differential voltage. I am powering the board at 3.3V from my Rapsberry Pi 4 and am using a GPIO pin on the same RPi 4 to provide the clock to the chip and then reading the DOUT on another RPi GPIO pin. Ground is provided by the RPi and is the same for the VDD ground and for the CLK and DOUT. I have CLKIN and DOUT hooked to an oscilloscope to see the DOUT signal with CLKIN.
The EVM has been powered for a while before I try to clock in information from DOUT. I leave the voltage unchanged and I send 16 clocks via CLKIN. I expect that I should get the same bit pattern back from DOUT every time I apply the same CLKIN sequence, but the signal read back from DOUT changes, sometimes greatly.
For example, when I try to clock in a DOUT reading I might get something like the folllowing.

But when I try it again with the same exact voltage I would get something like the following.

My assumption is that the DOUT signals should be identical with the same voltage
I have varied the input voltage to 0.9V, 0V, and -0.7V with similar results.
Am I doing something wrong in how I'm trying to read this? I would assuming bit-banging the CLKIN and then reading DOUT should work, am I wrong?
Please advise.