Part Number: DAC53204
Hi
I can't Find data on I2C VIH and VIL min and max levels when the DAC is supplied with 1.8V.
Please help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC53204
Hi
I can't Find data on I2C VIH and VIL min and max levels when the DAC is supplied with 1.8V.
Please help
Hi Alexander,
VIH and VIL digital input voltages are given in the recommended operating conditions table. The VIH and VIL values are the same for the 1.7V to 5.5V supply range.

For the I2C timing requirements, the given timings should be measured from VIL to 70% of VDD.


Best,
Katlynne Jones