Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256: Simultaneous Sampling

Part Number: ADS1256
Other Parts Discussed in Thread: ADS131A04, ADS131E08, ADS131M08

Hi sir,

Can this device do simultaneous sampling?  or not?
For example, if 8 identical waveforms are input in a single ended input,
Will different phases of analog-to-digital conversion timing deviate?

Thanks a lot.
Regards,

  • Hi Frank,

    The ADS1256 cannot measure multiple channels simultaneously. The ADS1256 is a multiplexed ADC, so there would be some phase difference between samples on different channels.

    If you want a 24-bit ADC, I would suggest looking at the ADS131E08 or ADS131M08 for a 24-bit, 8-ch, simultaneous sampling ADC. You could also use 2x ADS131A04.

    -Bryan