Part Number: ADS7924
Hi Team,
My customer is having an issue with the ADS7924 in that only CH0 reading is matching the real measurement.
The following were the I2C communications between the host PC to the ADS7924, used Manual-single mode.

Host PC reads:
vN13v0_code = 0x555
vN13v0 = 1.67 V.
iN13v0_code = 0x34A
iN13v0 = 1.03 V.
vP6v0_code = 0x505
vP6v0 = 1.57 V.
iP6v0_code = 0x23C
iP6v0 = 0.70 V.
However, the real measurement to the pins:
Pin 12 = CH0: 1.67V
Pin 11 = CH1: 1.61V
Pin10 = CH2: 3.0V
Pin 9 = CH3: 0.223V
Schematic:

Thanks,
Mitchell