Other Parts Discussed in Thread: AMC7904, AMC7924
We are evaluating the TI AMC7904 for our TDD application where we require to control Gate Bias of 8 FETs. We were considering use of two TI AMC7904 devices to control the 8 GAN FETs.
To Save Space in RF section, we are evaluating if the two Drain Supply Switches (High current PMOS switch) which are controlled with the PA_ON signal of the AMC7904, can be replaced with a single Drain Supply Switch common to all 8 PA GAN FETs.
- Need to understand if the above configuration will be supported by the two AMC7904 devices?
- Can we combine the PA_ON control outputs of the two AMC7904 to control single Drain Supply Switch for the 8 PA GAN FETs?
- In this case will the Power up and down sequencing of all the 8 PA GAN FET be complied with?
- Please let us know your suggestion for this?
We considered the AMC7924. However from checking the datasheet, we do not see support for TDD Switching control which we can see in the AMC7904 device.