This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7843: Initial settings

Part Number: ADS7843

Hi support team.

I  have some question from my customer below.

- Are settings immediately after startup of PD0 / PD1 "00" or "11"?

  I would like to know the initial settings of PDx.

- Is there a limit to the VCC startup time?

- The maximum frequency of DCLK is 2.5MHz, is it correct?

I appreciate if you give me some info to me.

Best regards,

Higa