Other Parts Discussed in Thread: ADS1115
Hi,
Doubt 1.May I get the testing code of ADS1114 (like Arduino or Raspberry Pi )…?
Doubt 2.The slave address of ADS1114 has (0x48 - ADDR connected GND ; 0x49 - ADDR connected to VCC- 5V) Is this the right slave address …?
Doubt 3. I have tested ADS1114 (ref. while browsing ) Arduino : I connected the A0 and A1 pin simultaneously to 5v or Gnd Sometimes I'm getting the data but not constantly and either one pin connect to VCC and another to GND the value doesn't changing. What was the issues in that....?