Part Number: ADS130E08
Other Parts Discussed in Thread: ADS131A04
Hi Team,
I want measure the current values from power line for my project. I need to have a sampling rate of maximum 5ksps and simultaneous sampling of 3 channels , So I choose ADS130E08 for my application. But while reading the data sheet of the same I find it is hard for me to understand the concept of differential input. Could you please give me an explanation on this. If I want measure a current in the range 0-30A rms from mains how should I decide the CT and input voltage to Analog pins of this ADC. And what is the concept behind common mode voltage at input? if I am using a reference 2.4V internal and AVDD 3.3V and PGA gain 1 what will be the limits of my analog input. In datasheet it is shown FSDI 4.8V what it means? Do I need give DC bias AC signal at ADC input?
Regards,
Vineeth