Hi,
I'm using a load cell with these specifications:
Full-scale load: 4400N
Rated Output; 4.5mv/v
Excitation: max 15.
ADC res, 24 Bit
I want to have a minimum 10N accuracy. I connected to excitation to a 2.5V accurate reference voltage. The ADC reference voltage(max 1.3v) is supplied from another accurate 1.2V. (LT6658).
I know that this is not a radiometric reading. But I'm confused about how can I convert the ADC value to the analog voltage.
For example, for a 22N weight, the ADC value is 162. Is the below formula is correct?
(162/2^24)*1.2=11.58uV
should I use 1.2 v for this formula or 2.5V?
Thanks