Part Number: DAC7750
Dear Team,
I am using DAC7750 with a PIC controller.
The problem i see is that, when i power up the default current i get out is approx 50mA without configuring anything.
I could not establish communication as well. I always read a 0xFF or 0x00 sometimes rarely 0xFD from the control register after putting in some data.
I can inspect the communication part next with a oscilloscope, but the current out of 50 mA really worries me without doing anything. (added a 150E load resistor on the outputs and got a 8.9V across it)
Is there something i did wrong or any chances on how this can happen ?. I tried pulling the CLR pin directly to GND as well referring to the other schematics in the forum.
I tried it out with my another proto board as well, but both resulted in the same behavior.